Technical FAQs

Ask a Question

Does the M340 PLC maintian state ram during a power cycle?

Yes.  This is referred to as a "Warm Start" and the values are written to the Backup Zone at power down and then back to state ram at power up.


Was this helpful?
What can we do to improve the information ?