Technical FAQs

Ask a Question

What are the default user privilege levels in Power SCADA?

Issue
What are the default user privilege levels in PowerLogic SCADA/ Power SCADA

Product Line
Powerlogic SCADA 7.x
PowerScada Expert 8.x
PowerSCADA Operation 9.0

Environment
User creation. 

Cause
User wishes to create new users using the default user privileges. 

Resolution
There are 5 different default user privileges in PowerLogic SCADA / Power SCADA as per below.
Note: The privilege levels need to be manually with a role. They are not part of the project by default in most cases.  This privilege level also applies to Windows Active Directory logins. 

Access Right
User Levels / Global Privileges
Description
Operator1
Operator2
Engineer
Administrator
Kernel
 
2
4
6
7
8
Circuit Breaker, Switch control
 
X
X
X
X
Alarms acknowledgment
X
X
X
X
X
Alarm configuration
 
 
X
X
X
Add/remove log-in users
 
 
 
X
X
Shutdown Runtime    
X
X
X

Was this helpful?
What can we do to improve the information ?