Browse FAQs

Where can I download the latest version of the EM4800 Configuration Tool

Published date: 14 May 2019

Issue: 
User would like to install the EM4800 configuration tool

Product Line:
EM4800 Series Meters

Environment:
Meter configuration Software

Resolution:
Attached is the EM4800 Configuration Tool. Uninstall any prior version before installing v1.6.1.1154
The EM4800 tool is usable with both the EM4800 and E4800 meters.

Note: Regarding the use of the Meter Configuration tool in Windows 7, Version 1.20 Build 1046 of the EM4800 Configuration Tool which is shipped with the meter does not support Windows 7 Operating System. The attached version of the EM4800 Configuration Tool, Version 1.60 supports both .Net Framework v3.5 and the Windows 7 Operating System.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.