Technical FAQs

Ask a Question

Where can I download the latest version of ION Setup software?

Issue
Latest version of ION Setup software Installer is required.

Product Line
ION Setup 3.1.x

Environment
Software Installation Files

Resolution
The latest version of ION Setup is v3.1.19072.01 published on March 13, 2019.

The latest version can be downloaded using the link below:
ION Setup Software

The ION Setup Software, User Guide, and Device Configuration Guide can also be obtained by visiting link below
(Note: The latest version of ION Setup software may not be up-to-date from the link below):
ION Setup Software and Documents

For ION Setup 3.0 User Guide and Device Configuration Guide, refer to article FA346479

For ION Setup revision History and Features & Fixes, refer to article FA222043

ION Setup is only supported on Windows Vista and newer.1

Note that for the best compatibility, we strongly recommend that users run ION Setup on windows versions that are officially supported by Microsoft.
Kindly refer to the Microsoft link below for end of support information:

https://support.microsoft.com/en-us/lifecycle/search

Was this helpful?
What can we do to improve the information ?