Technical FAQs

Ask a Question

What do I need to connect the TSXETG1010 module to a Unitelway bus?

Issue: 
What is needed in order to connect the TSXETG1010 module to a Unitelway bus

Product Line:
TSXETG1010, Unitelway


Resolution:
To connect the TSXETG1010 module to a Uni-Telway bus, you need one of the following:
- The cable with product reference TSX ETZ CDN 003, supplied with the module, to establish a connection via a TSX P ACC01 box,
- The cable with product reference VW3A8306 to establish a connection via a TSX SCA 62 box,
- The cable with product reference VW3A8306D30 to establish a connection via a TSX SCA 50 box.


Was this helpful?
What can we do to improve the information ?