Browse FAQs

Is there a sample project on serial printing using the Script Driver in Vijeo Designer?

Published date: 10 May 2019

Issue: 
sample project on serial printing using the Script Driver in Vijeo Designer

Product Line:
Vijeo Designer


Resolution:
Yes, below is a sample project on serial printing using the Script Driver in Vijeo Designer.
Serial Printing.zip

**Please note** This project was created in Vijeo Designer V4.6D.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.