Technical FAQs

Ask a Question

Does the ETL / EGX300 logging tool work with ION Enterprise and StruxureWare Power Monitoring?

Issue
Does the ETL / EGX300 logging tool work with ION Enterprise, StruxureWare Power Monitoring and Power Monitoring Expert?

Product Line
IONE, SPM  and PME

Environment
Power Monitoring Software

Cause
Need to know if the ETL/EGX300 logging works with IONE, SPM and PME

Resolution
The EGX300 ETL package works with the following versions:

  • ION:E 6.0 or 6.0 sp1 (Note that ETL tool is not free with ION Enterprise 6.0 or 6.0 SP1.
  • One should contact sales to purchase the right version for ION Enterprise V 6.0 SP1)
  • SPM 7 or 7.0.1 and Power Monitoring Expert (PME)
Was this helpful?
What can we do to improve the information ?