Technical FAQs

Ask a Question

How can I determine if an ASP890300 will replace a P800 power supply

Issue:
How to determine power supply replacement.

Product line:
800 series and remote I/O.

Cause:
Obsolescence of product

Resolution:
You must determine the current draw of the I/O modules that are in your rack/drop to know if the ASP890300 is a direct replacement.  Use the 800 series I/O calculator attached below to determine your load on the rack/drop. This will help you determine if you need to add a 2nd supply in one of the secondary racks.

Note: The 800 series is obsolete and the recommended replacement for this would be either the M340 or the M580 with the x80 I/I. Contact your local distributor or Schneider Sales office for more information regarding this.
Was this helpful?
What can we do to improve the information ?