Browse FAQs

Where can I find instructions for ATV12 drive basic programming?

Published date: 31 July 2019

Issue:
Where can I find instructions for ATV12 drive basic programming?

Product line:
Altivar 12

Environment:
All models, all serial numbers
 
Cause:
Basic Programming for the ATV12 drive
 
Resolution:
Enter and scroll down to CONF.

CONF Menu:
ACC Acceleration
DEC Deceleration
LSP Low Speed (0-60Hz)
HSP High Speed 

Scroll down to FULL and press Enter.

DRC Menu:
(Set using motor's nameplate data)
BFR Standard Motor frequency (usually 60Hz)
UNS Rated Motor Voltage
FRS Rated Motor Frequency (usually 60Hz)
NCR Rated Motor Current (motor's FLA)
NSP Rated Motor Speed (in rpm's)
TFR Max Frequency (usually 60Hz)
CTT Motor control type

FUN Menu:
RRS Reverse assign
  CLI- (submenu)
  CLI Current limitation (120% of FLA for variable torque, 150% of FLA for constant torque)

I-0 Menu:
TCC 2/3 wire type (2C or 3C)
TCT 2 wire type control (LEL, trn, PFO)

FLT Menu:
Select tHt and press Enter
ITH Motor Thermal (match FLA)

Refer to the ATV12 Programming Manual BBV28581 or Getting Started with ATV12 S1A5614603 for further details.
:

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.