Technical FAQs

Ask a Question

What is the maximum rated DC current at DC voltage for the auxiliary contacts of C60.

The maximum rated DC Voltage and DC Current for the Category DC12 (IEC 60947-5) auxiliary contacts OF, SD, OF+SD/OF, OF.S (Reference - 26924,26927,26929,26923) of C60 MCB is as below:
 
 
DC Voltage DC Current
24V 6 A
48V 2 A
60V 1.5 A
130V 1 A
 
 
The maximum rated DC Voltage and DC Current for the Category DC13 (IEC 60947-5) auxiliary contacts OF special (Reference - 16940) of C60 MCB is as below:
 
DC Voltage DC Current
230V 1 A
 
Was this helpful?
What can we do to improve the information ?