Browse FAQs

What is the maximum angle at which CT Contactor can be mounted for normal operation.

Published date: 03 June 2019

The maximum angle at which CT Contactor can be mounted in relation to the normal vertical mounting plane from the rail is 45 degrees, for proper operation.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.