Browse FAQs

What is the maximum rated AC current at AC voltage for the auxiliary contacts of C60.

Published date: 03 June 2019

The maximum rated AC Voltage and AC Current for the Category AC12 (IEC 60947-5) auxiliary contacts OF, SD, OF+SD/OF, OF.S (Reference - 26924, 26927, 26929, 26923) of C60 MCB is as below:
 
 
AC Voltage
AC Current
380…415V
3 A
220…240V
6 A
 
 
The maximum rated AC Voltage and AC Current for the Category AC15 (IEC 60947-5) auxiliary contacts OF special (Reference - 16940) of C60 MCB is as below:
 
AC Voltage
AC Current
220…240V
6 A

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.