Browse FAQs

Does Lexium 05 servo drive support BMH motors?

Published date: 12 June 2019

No, BMH motors are not compatible with Lexium 05 drives due to the type of encoder that is used in these motors.
If a BMH motor is connected to a Lexium 05, the drive will display fault 7120 which indicates that invalid motor data has been read. 

rev 1-24-18

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.