Technical FAQs

Ask a Question

Does the 140NOC78000 have the PLC Program Viewer capability?

 

Title
140NOC78000 PLC Program Viewer
 
Issue
Explain requirements for 140NOC78000 support of the PLC Program Viewer.
 
Product Line
Modicon Quantum.
 
Environment
Unity Programming software version 7.0 or greater
140NOC78000 firmware version 1.61 or higher
 
Resolution
Yes, the 140NOC78000 module supports the PLC Program Viewer via its Default web pages. Requires that the associated the Unity  program have its Projects Settings set to enable the PLC Program Viewer and the Data dictionary  capability.
Was this helpful?
What can we do to improve the information ?