Browse FAQs

Do all NetShelter SX cabinets ship with the same key?

Published date: 11 June 2019

Issue:
A customer needs to know if all NetShelter cabinets ship with the same key.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Having a single key allows ease and simplicity for customers who own multiple cabinets. Or, someone may want unique keys on some cabinets.

Resolution:

Yes, all NetShelter SX cabinets ship with the same key for the front door, rear doors and side panels.The standard NetShelter SX replacement key is part number W870-8135. 
If you would like information on unique locks for NetShelter SX cabinets please see Knowledge Base document FA158606.http://www.apc.com/us/en/faqs/FA158606/ 
If you need replacement keys for a NetShelter cabinet other than the NetShelter SX please see Knowledge Base document FA158623: http://www.apc.com/us/en/faqs/FA158623/ 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.