Browse FAQs

What is the difference between the Momentum Interbus tophats 170INT11000 and the 170INT11003?

Published date: 16 April 2019

Issue:
To know the difference between the different INT tophats and capabilities.

Product Line:
Momentum

Environment:
All Software packages, Proworx, Modsoft, Proworx32, EcoStruxure Control Expert, (formally known as Unity Pro)

Cause:
Not seeing any of the diagnostics in the network.

Resolution:
The only difference between the two is that the 170INT11000 is SUPI2 and the 170INT11003 is a SUPI3 chip and this allows for diagnostics. They can be mixed and matched but if you are using all 170INT11003 and then install a 170INT11000 you will not be able to do the diagnostics with the network. The Interbus network will run as if all the nodes were 170INT11000 modules with no diagnostics.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.