Technical FAQs

Ask a Question

How many bonding points are on the NetShelter SX cabinet and where are they located? What are the dimensions of the holes?

Issue:
Installation requires the number of bonding points, their location, size and dimensions. 

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Cabinets need to be bonded to a common ground.

Resolution:
See attached file

Was this helpful?
What can we do to improve the information ?