Browse FAQs

What is the part number for the Ethernet IP / Modbus TCP IP option card for the ATV32 series drives?

Published date: 07 May 2019

Issue:
What is the part number for the Ethernet IP/Modbus TCP/IP option card for the ATV32 series drives?

Product Line:
Altivar 32 series drives.

Environment:
All models, All serial numbers.

Cause:
Part number unknown.

Resolution:
The part number for the combination Ethernet IP/Modbus TCP/IP card for the Altivar 32 series drives is VW3A3616

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.