Technical FAQs

Ask a Question

Is SYMax Programming software still available?

Issue:
Software for Sy/Max product

Product line:
Sy/Max

Environment:
Winmate SFW572

Cause:
No software to connect to the PLC.

Resolution:

The WinMate programming software, ordering part number 8010SFW572 can still be ordered through the Service Sales group. Simply send an email request to "service.sales@se.com" and ask for pricing and availability on the WinMate 8010SFW572 programming software.

For the programming cable, NR&D sells a SC902 Smart cable which is a SyMax compatible RS-422 cable with a miniature RS-232/RS-422 converter built into the 9-pin RS-232 end. It is intended to be used to connect the 9-pin RS-232 COM port of a personal computer directly to the SyMax compatible RS-422 port of the controller. To purchase the SC902 cable contact to NR&D (Niobrara Research & Development) at #800-235-6723.
 
Was this helpful?
What can we do to improve the information ?