Technical FAQs

Ask a Question

Can the VW3A1101 keypad be swapped between ATV61 and ATV71 drives?

Issue:
Can the HMI display be swapped between ATV61 and ATV71 drives?

Product Line:
ATV61  ATV71

Environment:
All

Cause: 
For Spare parts

Resolution: 
Yes, the VW3A1101 keypad is common to both ATV61 and ATV71 product lines and is interchangeable between them. To prevent an HMI comm fault when disconnecting the HMI, ensure that the drive is not in local control (being controlled by the HMI), but rather in terminal or comms control.
Was this helpful?
What can we do to improve the information ?