Technical FAQs

Ask a Question

REJECT - Can the Remote Keypad Display (IP65) VW3A1007 be used with a ATV212?

Issue:
Can the part number VW3A1007 be used with a ATV212?

Product Line:
Altivar 212 ATV212

Environment:
All

Cause:
None

Resolution:
Part number VW3A1007 is not compatible with ATV212.
VW3A1007  (IP65) is for use with ATV312, ATV12.     
 
VW3A1101 is the recommended remote keypad for use with ATV212.
Other components needed include:
VW3A1102 remote mount kit
VW3A1103 cover for IP65
VW3A1104R** cable available in several lengths
Was this helpful?
What can we do to improve the information ?