Technical FAQs

Ask a Question

Can I use the Vijeo Designer simulator to connect to the HMISCU Codesys to read data?

Issue:
Can I use the Vijeo Designer simulator to connect to the HMISCU Codesys to read data?
 
Product Line:
Magelis HMISCU, Vijeo Designer, Somachine
 
Resolution:
No, you can not use the Vijeo Designer simulator to communicate to the HMISCU's PLC side.  The reason for that is because in the Vijeo Designer I/O Manager, the Somachine driver does have a PLC address/node name.  Therefore the Vijeo Designer simulator will not be able to find the PLC.
Was this helpful?
What can we do to improve the information ?