Technical FAQs

Ask a Question

Can the ATV212 communicate Profibus?

Issue:
Can the ATV212 communicate Profibus?

Product Line:
ATV212

Environment:
All models and serial numbers

Cause:
None

Resolution:
Profibus is not offered as a communication option.  A third party like "Anybus" can provide a gateway option from Profibus to an ATV212 integrated protocol.

Was this helpful?
What can we do to improve the information ?