Technical FAQs

Ask a Question

What is the maximum number of 140NOC78000 modules in a Unity project?

 

Title
140NOC78000 Module
 
Issue
Explain the maximum number of 140NOC78000 supported in a Unity project.
 
Product Line
Modicon Quantum.
 
Environment
Unity Programming software version 7.0 or greater
140NOC78000 firmware version 1.61 or higher
 
Resolution
A maximum of four NOC78000 modules are supported in a Unity project.
Was this helpful?
What can we do to improve the information ?