Technical FAQs

Ask a Question

What is the Ethernet IP communication option module for the ATV32 drive?

Issue:
What is the Ethernet communication option module for the ATV32 drive?

Product Line:
ATV32

Environment:
All models
 
Cause:
Product Selection & Services

Resolution:
Part number  VW3A3616    Ethernet IP—Modbus™ TCP/IP daisy chain option card, two RJ45 ports 10/100 Mbps, half duplex and full duplex, embedded web server.
Was this helpful?
What can we do to improve the information ?