Technical FAQs

Ask a Question

Can the configuration done in SoMove be imported to the Altivar drive while it is running the motor?

Issue:
Can the program be backed up from the drive using SoMove while the drive is running?

Product Line:
All drives and soft starts

Environment:
All

Cause:
None

Resolution:
No, you cannot download from SoMove to the drive while it is running the motor.  This is the same as standard programming.  Most parameters cannot be changed whille the drive is running. 
You will have to stop the drive before doing that. 
You should be able to connect and load from the drive to SoMove while it's running.
Was this helpful?
What can we do to improve the information ?