Technical FAQs

Ask a Question

Where can I download SoMove software and the drive/soft starter DTM files?

Issue:
Where can I download SoMove software?

Product Line:
SoMove Software

Environment:
All

Cause:
Needs SoMove software and DTM files

Resolution:

Below are the Links for SoMove Software and DTMs for AC Drives and Softstarts.

DTM files will need to be installed for drive profile recognition prior to connection through Somove.
 
SoMove core software:
http://www.schneider-electric.us/en/download/document/SoMove_FDT/

DTM file for Altivar 600 series process drives                             
https://www.schneider-electric.com/en/download/document/ATV6xx_DTM_Library_EN/

DTM file for Altivar 900 series process drives 
http://www.schneider-electric.com/en/download/document/ATV9xx_DTM_Library_EN/

DTM file for all other supported Altivar series drives (includes ATV12, ATV31, ATV312, ATV32, ATV61, ATV71, ATV212)   
http://www.schneider-electric.com/ww/en/download/document/Altivar_DTM_Library

DTM file for Altistart 22 and Altistart 48 soft starters  
http://www.schneider-electric.com/en/download/document/Altistart_DTM_Library/

DTM file for Altivar 320:
https://www.schneider-electric.com/en/download/document/ATV320_DTM_Library/

DTM file for Altivar 340:
https://www.schneider-electric.com/en/download/document/ATV340_DTM_LibraryEN/

WinZip or 7-Zip Extraction software may be needed for compressed/zipped files. If needed you can Download Free version 7-Zip from;  http://www.7-zip.org/

 

Was this helpful?
What can we do to improve the information ?