Technical FAQs

Ask a Question

Created a Vijeo Designer project within Somachine v4.1, how come the simulation build is grayed out?

Issue:
Created a Vijeo Designer project within Somachine v4.1, how come the simulation build is grayed out?

Product Line:
Vijeo Designer, Somachine

Resolution:
If you installed Somachine v4.1 with Vijeo Designer v6.2, but only registered the license for Somachine, when creating a Vijeo Designer project outside of Somachine, you will not have an option to run the Simulation Build.  In order to run Simulation Build, you will need to a stand alone license for Vijeo Designer.
Was this helpful?
What can we do to improve the information ?