Browse FAQs

ATV61 or ATV71: What can cause a drive state of SOC?

Published date: 05 August 2019

Issue:
ATV61 or ATV71: Drive state shows SOC

Product Line:
ATV61 and ATV71

Environment:
All models and serial numbers

Cause:
Motor disconnected or motor windings are open.

Resolution:
SOC is shown as the drive state when a run command is issued and the Fault Management parameter Output Phase Loss is set to "Output cut".  The VFD will remain in this state until an electrical connection is made with the motor.  Then the VFD will begin output to run the motor.  The SOC indicates either the motor is not yet connected or there is a problem with the motor.  Check the motor and motor wiring.  Look for an open contactor or disconnect between the drive and motor.  Close the circuit where appropriate.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.