Browse FAQs

What are the basic wiring connections for the ATV212 drive?

Published date: 03 June 2019

Issue:
What are the basic wiring connections for the ATV212 drive?

Product line:
ATV212, Altivar 212

Environment:
All models

Cause:
Limited wiring details provided with the drive.

Resolution:
The minimum requirements to operate an ATV212 drive are a run command and a speed reference.  By default from the factory, terminals F to P24 are the run forward and run permissive input.  VIA to CC is the default speed reference for 0-10V. 

P24 has its own 24VDC power supply, so use a dry contact closure on F to P24. 

**Note these values and assignments can be changed in the Programming.  These are the default settings only, with CNOd = 0 and FNOd = 1.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.