Technical FAQs

Ask a Question

When did the ATV16 drive become obsolete?

Issue:
When did the ATV16 drive become obsolete?

Product line:
ATV16, Altivar 16

Environment:
All models.

Cause:
Determine age of unit, product obsolescence

Resolution:
The ATV16 became obsolete in 1996.  The current replacement is the ATV12 or ATV320, depending on the application.  There are some differences that should be reviewed by the customer such as wiring, dimensions, and ratings.
Was this helpful?
What can we do to improve the information ?