Browse FAQs

Do the DZ2 lug kits offered for the ATS22 softstarters include mounting hardware?

Published date: 04 June 2019

Issue:
Do the DZ2 lug kits offered for the ATS22 softstarters include mounting hardware?

Product Line:
ATS22 Altistart 22

Environment:
ATS22C11 through C59 models

Cause:
Hardware is required.  Is it provided with the lug kit?

Resolution:
The DZ2FH6 and DZ2FK6 lug kits do not include any lug mounting hardware.
The ATS22 does not include lug mounting hardware.
The installer needs to procure the hardware elsewhere.
The installation bulletin references the hardware required.  See the attached file.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.