Technical FAQs

Ask a Question

Where can I find the End User License Agreement for PME 7.2.2, PME8.1 and PME9 ?

Issue
The customer wants to read the End User License agreement before purchasing or installating Power Monitoring Expert (PME) 7.2.2

Cause 
The End User License Agreement is located on the setup DVD. 

Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.x
Power Monitoring Expert 9

Environment
PDF reader

Resolution

The End User License Agreement (EULA) associated with Power Monitoring Expert 7.2 can be found as an html file located in the setup folder on the DVD. The EULA is also available through Floating License Manager under Help --> End User License Agreement. Attached to this article is the EULA in 8 different Langauge in a pdf format.
For PME 9, you can find a copy in the PME System Guide.

NOTE: This copy of the EULA is provided for your convenience. The official version of this license agreement is embedded in the Power Monitoring Expert product. If there are any differences
between the two versions, the product version supersedes the version in the system guide.
Was this helpful?
What can we do to improve the information ?