Technical FAQs

Ask a Question

How many TCP connections do the PM5000 series meters support?

Issue
How many TCP connections do the PM5000 series meters support?

Product Line
PM5110
PM5340
PM5341
PM5320
PM5560
PM5563

Environment
Power monitoring

Cause
How many concurrent TCP connections do the PM5000 series meters support?

Resolution
The PowerLogic PM5100 series support only a single TCP connection. 

The PowerLogic PM5300 series support up to 3 concurrent TCP connections. 

The PowerLogic PM5500 series support up to 32 concurrent TCP connections. 
 
Was this helpful?
What can we do to improve the information ?