Browse FAQs

Error Installing ION Setup: IONSetup.exe is not a valid Win32 application.

Published date: 17 May 2019

Issue
When installing the latest version of ION Setup software on a Windows XP machine the error shown below is displayed.



Product
ION Setup 3.0 (latest software revision)

Environment
ION Setup installation on windows XP machine

Cause
The later software revision(s) of ION Setup 3.x are a 64 bit application and are not supported on a Windows XP machine.

Resolution
Unfortunately, the newest version of ION Setup is only supported on Windows Vista and newer, refer to knowledge base article FA212816 .

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.