Technical FAQs

Ask a Question

Files to gather when troubleshooting PowerChute Network Shutdown 3.1 and 4.x

Issue:
What files are needed to troubleshoot PowerChute Network Shutdown v3.1 and 4.x?

Product:
PowerChute Network Shutdown (PCNS) version 3.1 and 4.x

Environment:
All supported Windows and Linux OS (see compatibility chart)

 
Cause:
Troubleshooting
 
Solution:
A.  Gather these files and send to Schneider Electric Technical Support
error.log, EventLog.txt, VirtualizationFileStore.properties, pcnsconfig.ini, javaVersionFile.log
NOTE: VirtualizationFileStore.properties is only available with VMware and Hyper-V configurations
 
On Windows the default path is
C:\Program files\APC\PowerChute\group1
 
On VMware vMA or APC Appliance the default path is
/opt/APC/PowerChute/group1
  
NOTE: Other files may be needed at a later date and different files may be needed to troubleshoot installation issues.
 
 
 
Was this helpful?
What can we do to improve the information ?