Browse FAQs

Is there any way for the ATV630 drive to keep a running total of gallons pumped?

Published date: 10 May 2019

Issue:
Is there any way for the ATV630 drive to keep a running total of gallons pumped? 

Product Line:
ATV Process Drives

Environment:
All serial numbers for ATV Process Drives

Cause:
N/A

Resolution:
Yes this function existing on the ATV630 (Process Drive). 
You can find this information in: Display -> Pump Dashboard  select the tab "Process" and then it is labeled "Total Quantity".
It is also possible to reset the Total Quantity. To do that go to: Display -> Counter.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.