Browse FAQs

Does the ATV12 drive have a type 1 conduit kit option?

Published date: 10 May 2019

Issue:
Does the ATV12 drive have a type 1 conduit kit option?

Product Line:
ATV12, Altivar 12

Environment:
All

Cause:
Nema 1 rating kit.

Resolution:
The ATV12 drives does not have a Nema 1 conduit kit option available.
There are covers over the input and output power terminals, but this does not meet the NEMA 1 requirements.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.