Browse FAQs

Can the ATV212 drive run a synchronous motor?

Published date: 03 June 2019

Issue:
Can the ATV212 drive run a synchronous motor?

Product Line:
ATV212

Environment:
All serial numbers for ATV212

Cause:
N/A

Resolution:
Yes the ATV212 can run a synchronous motor?
Version V5.4IE53#14 Corrections/Evolutions is the only firmware that can work with this specification.
Limited to: 
Support of Synchronous Motor control law
Support of Scroll compressor functions
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.