Search FAQs
Rope pull switches XY2C - NISD UL certificate of the XY2CH, XY2CE, XY2CED & XY2CJ E.stop rope pull switches
Attached the NISD.E352710 UL certificate of our emergency stop rope pull switches XY2CH, XY2CE, XY2CED and XY2CJ.
This NISD category covers emergency stop devices, including emergency stop units and emergency stop buttons, intended to be installed in a machine control system to perform a Category 0 or Category 1 stop function as defined in ANSI/NFPA 79, "Electrical Standard for Industrial Machinery." The emergency stop actuator provided in these devices is a self-latching type. These devices have been investigated for their functionality in addition to fire and electric shock safety. ANSI is the American National Standards Institute and NFPA is the National Fire Protection Association. Requirements refer to theIEC 60947-5-5 "Low-Voltage Switchgear and Controlgear” standard
This NISD category covers emergency stop devices, including emergency stop units and emergency stop buttons, intended to be installed in a machine control system to perform a Category 0 or Category 1 stop function as defined in ANSI/NFPA 79, "Electrical Standard for Industrial Machinery." The emergency stop actuator provided in these devices is a self-latching type. These devices have been investigated for their functionality in addition to fire and electric shock safety. ANSI is the American National Standards Institute and NFPA is the National Fire Protection Association. Requirements refer to theIEC 60947-5-5 "Low-Voltage Switchgear and Controlgear” standard
Released for:Schneider Electric India
Attachment(s)
Explore more
Explore more