Technical FAQs

Ask a Question

Can a LC1F265 and a LC1F330 contactor be mechanically interlocked?

Product Line:
 
Tesys F Line Contactors and Accessories
 
Resolution:

Yes but they have to be vertically mounted.  The LC1F265 will be on the bottom and the LC1F330 will be on the top.  Use an LA9FH4G mechanical interlock.
 
Was this helpful?
What can we do to improve the information ?