Browse FAQs

On the Altivar ATV630 process drive, what does embedded control (PLC, RTU, HMI) mean?

Published date: 09 May 2019

Issue:
On the Altivar ATV630 process drive, what does embedded control (PLC, RTU, HMI) mean?

Product Line:
Altivar ATV630 process drive

Environment:
All

Cause:
PLC control? Does the drive have a built in PLC?

Resolution:
Embedded control by PLC means the process drive has a built in Ethernet TCPIP card that can be controlled over a PLC controller.
RTU control means modbus control.
HMI control means keypad or local control.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.