Technical FAQs

Ask a Question

How to connect an HMIGTO to a Micrologix 1400 PLC?

Issue:
How to connect an HMIGTO to a Micrologix 1400 PLC?

Product Line:
Magelis HMIGTO

Resolution:
The cable combination to use is: Dsub9 [PLC side] <-- XBTZ9730 + XBTZG999 + D25 to D9 Converter (generic) --> Dsub9 [HMI Side]

You can also use XBTZ9730 + XBTZG919



 
Was this helpful?
What can we do to improve the information ?