Technical FAQs

Ask a Question

What is the cable to connect a HMISTU to a Momentum PLC?

Issue:
What is the cable to connect a HMISTU to a Momentum PLC?

Product Line:
Magelis (HMISTU/HMISTO/XBTGT/XBTGK/XBTGH/HMIGTO/HMIGTU)

Resolution:
The cable diagrams listed in the Modbus RTU driver manual of Vijeo Designer for this connection are:

XBTZG939 + XBTZ9711 for RS232 Communication
VW3A8306R10 For RS485 Communication.
Was this helpful?
What can we do to improve the information ?