Technical FAQs

Ask a Question

Can EcoStruxure Web Services (EWS) client send control commands back to Power Monitoring Expert (PME) Server?

Issue:
While connecting to PME via an EWS client, customers might have concerns over what actions the EWS client can perform on the PME software and the meters connected to the software.

Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0

Environment:
EWS Client Configuration

Cause:
There might be concern over EWS client connecting to PME server and performing control actions such as resetting various values on a meter.

Resolution:

The only action a client can take is request data and acknowledge alarms. In order to have an external software send control commands through EWS to PME we would need an EWS client implementation in PME, which we do not have. We only have an EWS server in PME.
 
Was this helpful?
What can we do to improve the information ?