Technical FAQs

Ask a Question

Latest Firmware version of Com'X 200/210 and Natively supported device type in the Energy Server Com'X 200/210

Product Line
COM'X200 / EBX200
COM'X210 / EBX210
 
Environment
Ethernet Gateway supported devices
 
Resolution
The latest version of firmware for Com'X 200 is 3.5.53 and the Com'X 210 is 6.0.4. 
They can be downloaded from the following links:  
COM'X200 firmware
COM'X210 firmware
 
In addition, review the attached device list for the Natively Supported Device Types.

For instructions on how to upgrade the firmware, view article FA270261.
Was this helpful?
What can we do to improve the information ?