Browse FAQs

PME 7.2.2 web application HTTP error 500.19 - This configuration section cannot be used at this path.

Published date: 09 April 2019

Issue
Opening the PME web application in a web browser yields the following error.
 

Configuration error reads:

This configuration section cannot be used at this path. This happens when the section is locked at a parent level. Locking is either by default (overrideModeDefault="Deny"), or set explicitly by a location tag with overrideMode="Deny" or the legacy allowOverride="false".


Other notes:
  • All other parts of the PME system are functioning as normal - devices are connected in Management Console, and Vista is displaying real-time values.
  • Web application may have been working previously.

  • User may have re-installed Windows OS or IIS.

Environment
PME 7.2.2 web application, Windows OS

Cause
One of the Application Development features is not enabled.
This can happen when IIS or the operating system is re-installed or updated.

Resolution
If using Windows 7 or 8, open the Start menu and type "Turn Windows features on or off" into the search bar.
In the features window, open Internet Information Services > World Wide Web Services > Application Development Features
Enable all features and close the window.

If using Windows Server 2012, open Server Manager, then click Manage > Add roles and features.
Click next, then select the PME Server in the Server Selection window and click Next.
In the Server Roles window, expand Web Server (IIS) > Web Server > Application Development.
Ensure that the latest .NET and ASP.NET features are selected, as well as CGI, ISAPI Extensions and Filters, and Server Side Includes are selected.

Note: After doing the procedure outlined in this KB, the Web Application may return a new error - HTTP Error 500.21.
If this occurs, see KB FA271594.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.