Technical FAQs

Ask a Question

Latest firmware version for the energy server COM'X 510 (Version 6.0.4)

Issue
What is the latest firmware version for the Energy Server Com'X 510 ?
 
Product Line
COM'X 510
EBX 510

Environment
COM'X 510

Cause
The new firmware upgrade is needed
Resolution
As of 14/06/2019, the latest version of firmware for COM'X 510 is 6.0.4 and can be downloaded from the link below.
https://www.schneider-electric.com/en/download/document/ComX_510_v6.0.4/

Instructions for upgrading the firmware can be found from KB FA270261
 
Was this helpful?
What can we do to improve the information ?