Technical FAQs

Ask a Question

Video: How do I generate a diagnostic file for PME 7.2.x, 8.x or 9.0?

Issue
Technical Support or sales may request that a diagnostic file be generated for a PME 7.2.x, PME 8.x, or PME 9.0 system.

This diagnostic file provides information from the PME system that is useful for troubleshooting, and understanding the scope of the system.

Product Line
Power Monitoring Expert 7.2.x, 8.x, 9.0

Environment
Generating a diagnostic file for PME 

Resolution
The procedure for generating a diagnostics file is as follows. A video procedure can also be viewed below.

  1. Open the PME program installation folder. On a typical system, this is in C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert.

    WARNING - Modification of files in this folder, beyond what is outlined in this procedure, may affect operation of your PME system. Do not make any changes in the program installation folder beyond what is described in this procedure, unless instructed to do so by a tech support agent.
     
  2. Open the "Diagnostics Tool" folder and double-click Diagnostics Tool.exe. The Diagnostics Tool window will open.
  3. In the Product Selection drop-down menu, select the appropriate version of the PME system.
  4. Click the Browse... button to select the diagnostic file output location. By default, the diagnostic file will save to the desktop.
  5. Click Select All to run all of the Analysis Items.
    If the technical support or sales agent directs you to select specific items, select those items instead.
  6. Click Start Analysis. Once the analysis completes, a .cab diagnostic file will be saved to the specified output location. This location is set to the Desktop by default.
NOTE: The password, if prompted, for the system diagnostic report is "Schneider"

 
Was this helpful?
What can we do to improve the information ?