Technical FAQs

Ask a Question

What are pulse characteristics of the Extended Range Powerlogic Energy Meter?

Issue
Need the pulse characteristics of the Energy Meter (EME) to determine the compatibility of the input device.

Product Line
Powerlogic Energy Meter

Environment
Application requiring submetering device that produce and energy pulse (kWh) 

Resolution
*Warning:  Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.


The pulse output is a contact closure only - power must be supplied externally in the range of 5-24 V ac/dc, with a maximum load of 100mA.

The pulse output provides a contact closure for 200ms at each pulse time. Be sure the controller will accept this signal as an input. See marked location of the pulse out terminal in figure below.




 
Was this helpful?
What can we do to improve the information ?